{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Which operators can be mounted in a XACA pendant station?

Article available in these languages: Spanish

Issue:
Compatible operators for XACA pendant station

Product Line:
Harmony XAC

Environment:
Pendant control station XACA

Resolution:
All ZA2 non-illuminated operators can be mounted in the cover or the bottom except for 60mm mushroom buttons. Also 3 position selector switches can not be used in the bottom. There are no contact blocks that will work with the 3 position selector switch in the bottom. Pilot lights and the XACA booted operators can be mounted in the cover only.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: