{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Are the booted operators used on an XACA & XACB pendant stations the same?
Issue:
Confirm the XACA & XACB operator compatibility

Product Line:
XAC Standard Duty Pistol Grips, Enclosures, Contact Blocks

Environment:
Push Buttons and Operator Interface

Resolution:
No, XACA booted operators use the XACA941* booted operators. XACB use XACB91** and XACB92** booted operators, they are not interchangeable.

Schneider Electric Australia