{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Will an FAL or FHL breaker that has an electrical accessory such as shunt trip, undervoltage trip, auxiliary switch, or alarm switch fit into a standard FA enclosure?
Issue:
Need to know if my FAL breaker will install in an enclosure with an accessory installed in it.

Product line:
Molded case circuit breakers

Resolution:
Yes. These accessories are internal to the breaker frame and require no extra enclosure room.

Schneider Electric Australia