{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between the 9001K20 and the 9001K21?
Issue:
What single potentiometer operator with single pot should be used with 10 ohms?

Product Line:
Harmony Push Buttons

Environment:
Harmony 9001K potentiometer

Cause:
Product Features

Resolution:
The 9001 K20 is the operator only without the single pot. The 9001 K21 is the operator with the single pot.

Schneider Electric Australia