{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Video: Installing the 225 Amp Feed-through Lug Kit into NQ Panelboards. Is there documentation for installing a feed thru lug kit?

Issue:
225A Feed Thru Lug Kit for a NQ Panelboards

Product Line:
NQ Paneboards

Environment:
Application

Cause:
Ordering and Installing

Resolution:
The NQ Panelboard does have the option for Field installation of the NQFTL2L kit,  for (30, 42 ckt) interiors and the NQFTL2H for 54, 72. and 84 ckt interiors.

NOTE:
Boxes will NOT need to be changed out to larger sizes when using a 42 ckt Main lug, or Main breaker interior. All other interiors will require a larger boxes.
See pg 9-9; Tables 9.16 and 9.17 in DIG 176 Link below for Box size changes needed


http://editiondigital.net/publication/?i=150050&p=9



Instruction Bulletin for Installation is attached

Schneider Electric Australia

Attachment(s)

NQ 225 A Feed-Through Lug Kit Installation for NQ Panelboards.pdfNQ 225 A Feed-Through Lug Kit Installation for NQ Panelboards.pdf [3.87 MB]