How can we help you today?
What is the difference between an XVBC02 & XVBZ02?
Issue:
XVBC02 & XVBZ02 Difference
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony XVB 70 mm Tower Lights
Cause:
Product Features
Resolution:
The XVBC02 is a 3.94``h stainless steel (black matte finish) support tube. The XVBZ02 is an aluminum (black matte finish)tube with a tulip base ( all one piece) and replaces this stainless item . Another newer option is an XVBZ02A tube and tulip base which is silver aluminum .
XVBC02 & XVBZ02 Difference
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony XVB 70 mm Tower Lights
Cause:
Product Features
Resolution:
The XVBC02 is a 3.94``h stainless steel (black matte finish) support tube. The XVBZ02 is an aluminum (black matte finish)tube with a tulip base ( all one piece) and replaces this stainless item . Another newer option is an XVBZ02A tube and tulip base which is silver aluminum .
Released for:Schneider Electric Australia
Explore more
Category:
Explore more
Category: