{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number for the spacer used with the LC*D09 through LC*D32 Contactor and the GV2AF3 combination block when the GV2 Motor Circuit Protector is mounted on din rail and the contactor hangs below it?
Issue:
Identifying the spacer part number for use with a LC*D, GV2AF3, and GV2 device combination

Product Line:
Contactors and Starters IEC

Environment:
Tesys D contactors and GV manual starters

Cause:
Spacer required

Resolution:
Compensation plate catalog number GV1F03, requires 2 pieces snap together.

Schneider Electric Australia