{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the terminal identification numbers for the LADN22 auxiliary contact module?
Issue:
Terminal numbers designation for LADN22

Product Line:
Contactors and Starters-IEC

Environment:
Tesys Contactors and Overload Relays

Cause:
Product Features

Resolution:
Normally open contacts are 53/54 and 83/84; normally closed contacts are 61/62 and 71/72.

Schneider Electric Australia