How can we help you today?
What is the wattage on the DL1BA and DL1BL bulbs used in the XVA indicating banks?
Issue:
What is the power in watts on the DL1BA and DL1BL bulbs used in the XVA indicating banks?
Product Line:
Harmony Tower Lights
Environment:
Harmony XB4/ZB4 Metal Push Buttons
Cause:
Product Features
Resolution:
AC or DC
2.5W 12V DL1BA012
4W 24V DL1BA024
6.5W 24V DL1BL024
4W 48V DL1BA048
7W 110V DL1BA110
7W 120V DL1BL120
5W 160V DL1BA160
6W 260V DL1BA260
What is the power in watts on the DL1BA and DL1BL bulbs used in the XVA indicating banks?
Product Line:
Harmony Tower Lights
Environment:
Harmony XB4/ZB4 Metal Push Buttons
Cause:
Product Features
Resolution:
AC or DC
2.5W 12V DL1BA012
4W 24V DL1BA024
6.5W 24V DL1BL024
4W 48V DL1BA048
7W 110V DL1BA110
7W 120V DL1BL120
5W 160V DL1BA160
6W 260V DL1BA260
Released for:Schneider Electric Australia
Explore more
Category:
Explore more
Category: