{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between ZB4BZ2005 and ZB4BZ1905 are the mounting holes the same size?
Issue:
Are the mounting holes the same size in ZB4BZ2005 and ZB4BZ1905 ?

Product Line:
Push Buttons and interface operators

Environment:
Harmony Push Buttons

Cause:
Product Features

Resolution:
ZB4BZ1905 is 70 mm in diameter
ZB4BZ2005 is 72mm top to bottom X 40mm from side to side.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: