{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How many contacts blocks can be mounted on 9001 type K, SK and KX operators, push button and selector switch, non-illuminated or illuminated?
Issue:
What is the maximum number of contacts blocks can be mounted on 9001 type K, SK and KX operators, push button and selector switch, non-illuminated or illuminated?

Product Line:
30mm Push Buttons

Environment:
9001 K/SK/KW Operators

Cause:
Need to know answer before the parts are ordered.

Resolution:
Maximum Contact block usage: includes Type K, SK and KX
2 blocks mounted side by side only: Any 2,3 or 4 position spring return selector switch (non-illuminated, illuminated or keyed).
2 blocks mounted in tandem on one side only: Any 2 operator interlocked push button.
2 blocks mounted in tandem ( total of four blocks)`` Any selector push button, keyed push button, 2,3 or 4 position maintained selector switch (non illuminated, illuminated or keyed), push-pull operators (non illuminated or illuminated), joy stick, dual push button.
3 blocks mounted in tandem (total of six blocks): Single momentary push buttons (non illuminated or illuminated).

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.