How can we help you today?
Will the XALD control station push button operators accept boots?
Issue:
Available boots for XALD control station push button operators.
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony Control Stations
Cause:
Product Features
Resolution:
Yes, clear boots are available for pushbuttons with circular heads. They are available in neoprene using catalog number ZBP0. For use in the food and beverage industry, they are available in silicone using catalog number ZBP0A.
Available boots for XALD control station push button operators.
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony Control Stations
Cause:
Product Features
Resolution:
Yes, clear boots are available for pushbuttons with circular heads. They are available in neoprene using catalog number ZBP0. For use in the food and beverage industry, they are available in silicone using catalog number ZBP0A.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: