{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What was a unitized EZ Stack meter center?

Issue:
Product Features

Product Line:
Unitized EZ Metering Equipment

Resolution:
The unitized EZ Stack devices were self-contained meter centers, available with up to six disconnecting means. The 100 A devices accepted field installed QO or Q1 tenant breakers. The 125 and 150 A devices were supplied with factory installed Q2 tenant breakers. This product line is obsolete. The current offering for this application would be MP METER-PAK.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: