{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between the 9001KM1L* and the 9001KM38L* which both are listed for 120 volts?
Issue:
Checking on the difference between the 9001KM1L* and the 9001KM38L*, both are listed for 120 volts.

Product Line:
9001KM Light Modules

Environment:
Push Button and Operator Interface

Cause:
Product Features

Resolution:
The 9001KM1L* is a transformer style light module with a 6 volt LED lamp for 120 volt AC input. The 9001KM38L* is a resistor style light module with a 12 volt LED lamp for 120 volts AC or DC input.

Schneider Electric Australia