{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is there an XB4 or XB5 push to test pilot light?
Issue:
Are push to test pilot lights available for 22mm?

Product Line:
Harmony Pushbuttons

Environment:
XB4 and XB5

Resolution:
Yes, the push to test pilot lights are available.  You will find selections in the new catalog.
XB4 (metal type)
https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=DIA5ED2121212EN.pdf&p_Doc_Ref=DIA5ED2121212EN
XB5 (plastic type)
https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=DIA5ED2121213EN.pdf&p_Doc_Ref=DIA5ED2121213EN

Before these push to test pilot lights made available in 22mm operators, the suggestion was using an illuminated pushbutton with (1) NO and (1) NC contact. The normal pilot light circuit is wired through the normally closed contact, and the test circuit is wired through the normally open contact. Customer will also have to jumper between the contacts.

Schneider Electric Australia