{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do you connect to UL 1077 Comb Bus Bars # 10285, 10286, or 10287?
Issue:
How to wire comb busbars 10285, 10286, or 10287

Product Line:
Multi-9 Circuit Breaker accessories

Environment:
Molded Case Circuit Breakers

Cause:
Cannot find equivalent to insulated connectors used with UL 489 and IEC comb bus bars. Need to know how the UL 1077 comb bus bars are wired.

Resolution:
Field wiring is applied directly to the comb bus bar by inserting both the wire and the tooth of the comb bus bar into the same box lug of the Multi-9 breaker. Alternatively, an appropriately sized breaker applied to the busbar can be backfed to power the bus.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.