{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the replacement part for the trip unit interlock of a Masterpact NW breaker?
Issue:
Broke the white trip unit interlock behind the trip unit.  Masterpact NW. NW breaker trips when it OPENS and red button pops out but no Ap light comes on.  Does not trip when it closes.

Product Line:
Masterpact NW

Resolution:
Replace the trip unit base, part number 47947. This part is available only to Square D/Schneider Electric Field Services and they must do the installation.

Schneider Electric Australia