{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Parts needed to upgrade a Masterpact NW breaker from a Micrologic 3.0 or 5.0 to the 3.0A, 5.0P, 6.0P, 5.0H, or 6.0H trip units
Inquiry:
Which parts are needed to upgrade a Masterpact NW breaker from a standard trip unit to a Micrologic 3.0A 5.0P 6.0P 5.0H or 6.0H?

Product Line:
Masterpact NW

Resolution:
Both fixed and drawout breakers need connector S33101 and the trip unit:
3.0A S141A
5.0A S143A
6.0A S144A
5.0P S163A
6.0P S164A
5.0H S173A
6.0H S174A

A neutral CT is required if the breaker is applied on a 4-wire system and new trip unit is a 6.0A, 6.0P, or 6.0H.
A neutral CT is also required if the breaker is applied on a 4-wire system and the new trip unit is a 5.0P or 5.0H being used for ground fault alarm.
See attached table for catalog numbers.

Fixed circuit breakers also need the following parts in addition to connector S33101:
External Voltage Sensing S47506 (P and H trip units only, if voltage sensing is required)
Secondary Disconnects (3) S47075 and (1) S47074
BCM S47405 (if Modbus is required)

Drawout circuit breakers also need the following parts in addition to connector S33101:
External Voltage Sensing S48533 (P and H trip units only, if voltage sensing is required)
Secondary Disconnects (3) S47850 and (1) S47849
BCM S48384 (if Modbus is required)

To upgrade from Ammeter to Power or Harmonic trip unit
Breakers with an Ammeter trip unit already have these parts, S33101 and the secondary disconnects.  The BCM and External Voltage Sensing kits are still required if communications and voltage sensing is desired..

Schneider Electric Australia

Attachment(s)
Neutral CT Table from 0613IB1607.pdf [45.32 KB]
Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: