{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is part number for a potentiometer for the 22mm potentiometer operators?
Issue:
Separate part number for 22mm Potentiometer.

Product Line:
Push Buttons and Operator Interface

Environment:
22 mm Harmony Push Buttons

Resolution:
Potentiometers are customer supplied.
They can be purchased at an electronics supply house. The operators are for potentiometers with a standard shaft length of 44 to 50 mm, and for the ZB4BD912 a shaft diameter of 6mm and for the ZB4BD922 a shaft diameter of 6.35mm.

Another option is to get the complete assembly (Operator + Potentiometer) Please see below for products part numbers.

+/- 10% linear mode precision complete potentiometer with screw terminals.

For METAL:
Resistance (k Ohms)WeightCatalog Number
10.095/0.209XB4BD912R1K
4.70.095/0.209XB4BD912R4K7
100.095/0.209XB4BD912R10K
470.095/0.209XB4BD912R47K
1000.095/0.209XB4BD912R100K
4700.095/0.209XB4BD912R470K


​For PLASTIC:

Resistance (k Ohms)WeightCatalog Number
10.048/0.106XB5AD912R1K
4.70.048/0.106XB5AD912R4K7
100.048/0.106XB5AD912R10K
470.048/0.106XB5AD912R47K
1000.048/0.106XB5AD912R100K
4700.048/0.106XB5AD912R470K

Schneider Electric Australia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: