{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the lug torque specification for a Powerpact J frame circuit breaker?
Product Line:
Circuit Breakers

Resolution:
The standard Al/Cu lugs are rated at 225 lb-in and require a 5/16 in hex bit torque wrench. See below for lug information.
The AL175JD (150 - 175 A) is 225 lb - in.
The AL250JD (200 - 250 A) is 225 lb - in.
The CU250JD (150 - 250 A) is 250 lb - in

See instruction bulletin, 48940-221-02

Schneider Electric Australia