{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What safety category rating do the CAD TeSys relays meet under IEC EN954-1? Do they have linked contacts?
Issue:
Safety category listing of CAD TeSys relays

Product Line:
Relays

Environment:
TeSys D Relays

Resolution:
​The Tesys CAD32** and the CAD50** relays and top mounted adder decks have positively guided or linked contacts.  Therefore the contacts meet IEC EN60947-5-1 and are approved to use in safety systems through category 4.

Schneider Electric Australia