How can we help you today?
What Is The Part Number For The Socket For RPM Relays?
Issue:
Identify a socket for RPM1*, RPM2*, RPM3*, and RPM4* relays
Product Line:
RPM Zelio Relays and Timers
Environment:
Relays and Timers
Resolution:
Please see table below.
[16] The inputs and outputs are mixed on both sides.
Identify a socket for RPM1*, RPM2*, RPM3*, and RPM4* relays
Product Line:
RPM Zelio Relays and Timers
Environment:
Relays and Timers
Resolution:
Please see table below.
Contact Terminal Arrangement | Connection | For Use with Relays | Catalog Number |
Mixed[16] | Screw terminals | RPM1••• | RPZF1 |
RPM2••• | RPZF2 | ||
RPM3••• | RPZF3 | ||
RPM4••• | RPZF4 |
[16] The inputs and outputs are mixed on both sides.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: