{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: Where is the wiring diagram located and what information does it contain and where is the date code located on ALL the molded case circuit breaker enclosures?
Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Resolution:
NOTE: This information will generally apply to ALL the Molded Case Circuit Breaker Enclosures(The F-frame, B-Frame, H-frame, the J-frame, the L-frame, the M-frame and P-Frame). But for the video a J250S was used.




The wiring diagram on the circuit breaker enclosures will be located on, one of the inside sidewalls of the enclosure. All the necessary information for the enclosure will be on the wiring diagram and will contain the following;
1) Catalog and series number of the enclosure
2) What type of Circuit breakers that can be used
3) Any accessory that can be used in the enclosure, like the solid neutral and equipment ground kit
4) The UL listed catalog number Prefixes for the breakers that can be used in the enclosure
5) Maximum wire sizes for the enclosure(NOTE: Sometimes the breaker can accept larger wire, BUT the enclosure wire bending space will be limited to what the wiring diagram shows)
6) The Wiring schematics
7) The Short Circuit Current Rating information for each breaker at each voltage level
8) The Date code. The date code will be an ink stamp, generally located on the inside back wall of the enclosure. The Date Code will be a 5 or 6 digit code and will read as follows; first two digits = year, the 2nd two digits = week of the year, the 5th digit = the day of the week and the last digit(if used) = the shift. For example, 183241 is year - 2018, week of year -32, day of week - 4 and shift - 1. (Aug. 9th, 2018)

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: