How can we help you today?
What is the NEMA rating of an XALD pushbutton enclosure?
Issue:
XALD pushbutton enclosure NEMA rating
Product Line:
IDSIG - Control and signalling
Environment:
XALD
Cause:
Product features and ratings
Resolution:
The XALD enclosures are all rated NEMA 1, 4X, 12, 13, and IP65.
XALD pushbutton enclosure NEMA rating
Product Line:
IDSIG - Control and signalling
Environment:
XALD
Cause:
Product features and ratings
Resolution:
The XALD enclosures are all rated NEMA 1, 4X, 12, 13, and IP65.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: