How can we help you today?
What are the stand alone short circuit current ratings on the LC1D** contactors?
Issue:
Tesys D SCCR
Product Line:
Contactors and Overload Relays
Environment:
TeSys™ D Contactors and Overload Relays
Resolution:
The contactors have a stand alone withstand rating that has been established by UL and is based on the maximum horsepower rating for a given device. However, only combination type starters are supplied with short circuit protective devices having a short circuit current rating.
They are as follows:
Horsepower SCCR (A)
0 thru 1 1,000
1 thru 50 5,000
51 thru 200 10,000
201 thru 400 18,000
401 thru 600 30,000
601 thru 900 42,000
901 thru 1600 85,000
1601+ 100,000
Tesys D SCCR
Product Line:
Contactors and Overload Relays
Environment:
TeSys™ D Contactors and Overload Relays
Resolution:
The contactors have a stand alone withstand rating that has been established by UL and is based on the maximum horsepower rating for a given device. However, only combination type starters are supplied with short circuit protective devices having a short circuit current rating.
They are as follows:
Horsepower SCCR (A)
0 thru 1 1,000
1 thru 50 5,000
51 thru 200 10,000
201 thru 400 18,000
401 thru 600 30,000
601 thru 900 42,000
901 thru 1600 85,000
1601+ 100,000
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: