{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: How do you panel mount the TeSys D-line contactors?
Issue:
LC1D09-D32 Panel mounting

Product Line:
IEC Contactors and Starters

Environment:
TeSys D-line contactors

Cause:
Panel mounting a D-line contactor

Resolution:
There are screw holes in the bottom, upper right and lower left corners of the contactor which must be extracted with a small screwdriver.

Schneider Electric Australia