How can we help you today?
9007C54B2 and 9007C68T10 - are these the same size and same operation?
Issue:
9007C54B2 and 9007C68T10 - are these the same size and same operation?
Product Line:
Limit Switches
Environment:
North American Products
Resolution:
Both are the same size, but operation is very different. 9007C54B2 has 1NO/1NC contact; contacts change state when arm moves either CW or CCW.
Head can be configured in the field to operate in CW trip, CCW reset; or CCW trip, CW reset.
9007C68T10 has 2NO/2NC with neutral position. 1 pair changes state when going CW, resets on return to center. The other pair changes state when going CCW, resets on return to center.
9007C54B2 and 9007C68T10 - are these the same size and same operation?
Product Line:
Limit Switches
Environment:
North American Products
Resolution:
Both are the same size, but operation is very different. 9007C54B2 has 1NO/1NC contact; contacts change state when arm moves either CW or CCW.
Head can be configured in the field to operate in CW trip, CCW reset; or CCW trip, CW reset.
9007C68T10 has 2NO/2NC with neutral position. 1 pair changes state when going CW, resets on return to center. The other pair changes state when going CCW, resets on return to center.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: