How can we help you today?
What is the function of the LUFDA10 Tesys U module?
Issue:
Tesys U function modules. how does LUFDA10 work?
Product Line:
Contactors and Starters-IEC
Environment:
TeSys™ U Open Motor Starter
Resolution:
It provides indication between an overload trip and a short circuit trip. It also provides for remote or automatic reset after a thermal fault.
Tesys U function modules. how does LUFDA10 work?
Product Line:
Contactors and Starters-IEC
Environment:
TeSys™ U Open Motor Starter
Resolution:
It provides indication between an overload trip and a short circuit trip. It also provides for remote or automatic reset after a thermal fault.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: