{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What the difference is between these 2 contact blocks - LADN22 and LADN22G?

Issue:
Identifying differences in two part numbers

Product Line:
IEC contactors and starters

Environment:
Tesys D Auxiliary contacts

Cause:
Determining which part number to order

Resolution:
They both have 2 normally open (N.O.) and 2 normally closed (N.C.) contacts.
The sequence and numbering are different
LADN22 from left to right read : N.O. 53 and 54; N.C. 61 and 62; N.C. 71 and 72; N.O. 83 AND 84.

LADN22G from left to right read : N.C. 31 and 32; N.C. 41 and 42; N.O. 53 and 54; N.O. 63 and 64.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: