How can we help you today?
What is the function of the LUFC00?
Issue:
Identify the function of the LUFC00
Product Line:
TeSys U Starters
Environment:
IEC Contactors and Starters
Resolution:
The LUFC00 is a parallel wiring module that you can install in your U-line starter so that you can connect the starter to your PLC I/O modules quickly and without any need for tools. It allows for energization of the coil circuit of each power base, and an output signal from a PLC. It also provides a `RUN` and `FAULT` status of each power base to the PLC. You can even tie each starter base to a LU9G02 splitter box via the RJ45 connect and have the splitter feed to the PLC.
Identify the function of the LUFC00
Product Line:
TeSys U Starters
Environment:
IEC Contactors and Starters
Resolution:
The LUFC00 is a parallel wiring module that you can install in your U-line starter so that you can connect the starter to your PLC I/O modules quickly and without any need for tools. It allows for energization of the coil circuit of each power base, and an output signal from a PLC. It also provides a `RUN` and `FAULT` status of each power base to the PLC. You can even tie each starter base to a LU9G02 splitter box via the RJ45 connect and have the splitter feed to the PLC.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: