{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What size cable does a LAD7B10 accept?
Issue:
Need to know the size cable accepted by the LAD7B10 block.

Product Line:
TeSys D overload relays

Environment:
IEC Contactors and starters

Cause:
Identifying cabling requirements.

Resolution:
It takes either a 1 flexible cable without cable end size 14-8 AWG or 1 flex cable with cable end size 16-12AWG or 1 solid cable without cable end size 16-10 AWG.


Schneider Electric Australia