{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the Part Number for the Mechanical Interlock for the 4-pole LC1DT20, LC1DT25, LC1DT32, and LC1DT40 Contactors?
Issue:
Four-pole IEC contactors needs the part number for the mechanical interlock

Product Line:
IEC Contactors

Environment:
Tesys D contactors

Resolution:
LADT9R1 is the mechanical interlock and power wiring only. The LADT9RV1 also includes an electrical interlock (2 NC contacts).

Schneider Electric Australia