{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number for the screws for the vented covers on a 400a and 600a NQ panelboards?
Issue:
What are the screws used for the vented covers on a the 400 and 600 amp NQ panelboards?

Product Line:
Panelboards

Environment:
NQ panelboards

Cause:
Product features

Resolution:
Use a LP9502 kit of 8 screws that includes captive hardware

Schneider Electric Australia