{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the NEMA rating of the S32598 and S32600 extended handle for the L frame breaker?

Product Line:
Circuit Breaker Accessories
PowerPact L

Environment:
Electrical Distribution Equipment

Resolution:
The S32598 and S32600 handles can be marked Type 12, and it is in UL file E103955, volume 3, section 8.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: