{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the difference between the LUCA32** and the LUCB32**?

Issue:
Identifying products differences

Product Line:
TeSys U Combination Motor Controller

Environment:
Product Characteristics

Resolution:
The LUCA32 is a standard control module that provides 3 phase, class 10, solid state overload relay protection along with the coil circuit. When the starter is also equipped with a communications module, the LUCA32 can accept run commands via the network.

The LUCB32 is an advanced control module and also provides 3 phase, class 10,  solid state overload relay protection and control coil but  also provides additional data via the network communication module.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: