{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How is the comms address set on a Micrologic ammeter or energy trip unit for H, J, and L frame breakers?
Issue:
How to set the comms address on a Micrologic ammeter or energy trip unit?

Product Line:
Micrologic  5.2A, 5.2E, 5.3A, 5.3E, 6.2A, 6.2E, 6.3A, 6.3E trip units

Resolution:
The comms address is set on the Modbus communication interface module (IFM) with blue dials. The IFM is external to the breaker and is mounted on a DIN rail.
This module, required for connection to the network, contains the Modbus address (1 to 99) declared by the user using the two rotary switches on the front. It automatically adapts (baud rate, parity) to the Modbus network in which it is installed. It is equipped with a lockout switch to enable or disable operations involving writing to the Micrologic trip unit, (such as reset, counter reset, setting modifications, and device opening and closing commands). There is a built-in test function to check the connections of the Modbus communication interface module with the Micrologic trip unit and front display module.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.