undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the part code for a 3 Phase 32A 30mA RCBO?

We do not offer a single 3 Pole 32 Amps 30mA RCBO.

You can use 3 Pole 32 Amps iC60 MCB and connect it with the 3 Pole Add-on Vigi Module "A9V02763" (comes with the neutral tail to be connected with the distributed neutral) - this combination is 6 Poles wide

If balanced three phase system with out neutral you should use Add on Vigi "A9V51363" - this combination is 6½ Pole wide

Schneider Electric Australia