{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number for Masterpact NW mounting brackets?
Issue:
What is the part number for Masterpact NW mounting brackets?

Product Line:
Masterpact NW

Resolution:
Mounting brackets come standard with the fixed mounted NW breaker.
The kits contain a set of 2 brackets.
There are two types of kits available: horizontal and vertical.
Horizontal Mount: S47828
Vertical Mount: S47829

Schneider Electric Australia