How can we help you today?
Are the XB5R and XB4 Wirless Push Buttons rated for CLASS 1 DIV 1?
Issue:
XB5R Wirless Push Buttons Ratings
Product Line:
Operator Interface Push Buttons
Environment:
All type XB5 Push Buttons
Cause:
In an environment where there might be explosive liquid or gas
Resolution:
It is not rated for Class 1 Division 1 or 2
It is rated for NEMA1,3R,4,12
IP40,IP55, IP65
XB5R Wirless Push Buttons Ratings
Product Line:
Operator Interface Push Buttons
Environment:
All type XB5 Push Buttons
Cause:
In an environment where there might be explosive liquid or gas
Resolution:
It is not rated for Class 1 Division 1 or 2
It is rated for NEMA1,3R,4,12
IP40,IP55, IP65
Released for:Schneider Electric Australia
Explore more
Category:
Range:
Explore more
Category:
Range: