{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Is the 9013F compatible with Skydrol?

Issue:
Is the 9013F compatible with Skydrol?

Product Line:
Pressure switches

Environment:
9013F

Cause:
Material comparability

Resolution:
It is not recommended for Skydrol.  Nitrile is the standard material used in diaphragm for the 9013F devices. The 9012G has an option to use ethylene propylene, form Q3, for the diaphragm.

Note that 9012G switches are control devices and cannot support inductive loads directly, but require an interposing contactor.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: