{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is a shunt trip coil and a closing coil automatically included when you order a Masterpact NT/NW or Powerpact P breaker with a spring charging motor?
Issue:
Do you have to select a shunt trip coil and a shunt close coil for Masterpact NT/NW or Powerpact P when they are motor operated? It is not very clear in the product selector.

Product Line:
Circuit Breakers

Resolution:
Masterpact NT or NW (electrically operated)
In the product selector, when you choose the option "Spring Charging Motor", the shunt trip and the closing coils are not automatically included for Masterpact NT and NW. You must select each one. You can have them all at the same voltage or different voltages. Note there is an option to add a second shunt trip, which can be at a different voltage than the others.

Powerpact P (electrically operated)
In the product selector, when you choose the option "Spring Charging Motor", the shunt trip and the closing coil are automatically included for Powerpact P. You don't select them. All three (motor, shunt trip, closing coil) will be at the same voltage. The shunt trip shown in the selector is for a 2nd shunt trip that is not involved in the electrical operation of the breaker. The 2nd shunt trip can be at a different voltage than the others.

Schneider Electric Australia