{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: How do I set a PowerPact or Masterpact circuit breaker with a Micrologic trip unit to a different specified amperage?
Issue:
How to adjust PowerPact P or R or Masterpact circuit breakers with Micrologic trip units to a different Amp rating?

Product Line:
PowerPact P, PowerPact R, Masterpact NW, Masterpact NT

Resolution:
The attached spreadsheet gives you the sensor plug and Long Time (rating plug) settings that will set the breaker to any amperage within its range.
Note that many amp settings can be attained with more than one rating plug and sensor combination.

Sensor plugs can be changed to a lower amperage in some cases; they cannot be increased from the original size, but they can be reduced as much as 50%.
It is not possible to put a 100A or 250A sensor in a 400A or larger breaker.  400A and larger breakers cannot accept 100A or 250A sensors.
See circuit breaker section of the digest for a chart showing possible sensor plugs for breakers 3200A and under.
Sensor Plug Replacement Guide attached includes references for amperages above 3200A.

Schneider Electric Australia

Attachment(s)
Sensor Plug Replacement 48049-145-03.pdf [494.1 KB]
Micrologic Amp Calculator3.xlsx [208.44 KB]