{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: Disabling Ethernet Network Connectivity on TeSys T Motor Management System

Article available in these languages: Spanish

Issue:
How to disable Ethernet Network connectivity in Tesys T controllers?

Product Line:
IEC Contactors and Overload relays

Environment:
Tesys T motor management system

Resolution:
There is no setting in the software to disable the ethernet network. On the Tesys T you actually use hardware to disable the network. There are two dials on the face of the device, a Tens dial and a Ones dial. On the Ones dial, choose the Disabled setting and then power cycle the Tesys T. The device will no longer look for a network and will not give the Network settings warning.


Schneider Electric Australia