{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is a XCSZP7012?

Product Line:
Machine safety switch

Cause:

Purchasing and identification

Resolution:

This is the switch portion of a coded magnetic switch. The switch will be marked with the XCSZP7012 part number but it is not sold without the magnet.
Complete part number for the switch with magnet is XCSDMP7012.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: