How can we help you today?
Why is the LCD display screen blank on a Micrologic Power or Harmonic type trip unit on a Powerpact P frame, R frame, or Masterpact circuit breaker?
Issue:
Why is the display blank on the trip unit?
Product Line:
Powerpact P frame, Powerpact R Frame, Masterpact NT, Masterpact NW
Resolution:
The LCD display on a Micrologic P or H trip unit will be blank unless the trip unit is energized. Energization requires one of the following sets of conditions:
Why is the display blank on the trip unit?
Product Line:
Powerpact P frame, Powerpact R Frame, Masterpact NT, Masterpact NW
Resolution:
The LCD display on a Micrologic P or H trip unit will be blank unless the trip unit is energized. Energization requires one of the following sets of conditions:
- The trip unit is energized by an external 24 Vdc applied to terminals F1-F2 (F1 negative-F2 positive). See attachment for location of terminals.
- The trip unit is energized by an FFTK or HHTK test kit
- There is at least 100 V between two phases, AND the load reaches approximately 20% of the breaker's rated current.
- Note that the display will not power up with primary injection testing unless one of the conditions in bullet 1 above is met.
- Note that Ammeter trip units do not require external power and the display will come on with sufficient current flow alone.
Micrologic 2.0A, 3.0A, 5.0A, and 6.0A Electronic Trip Units
Micrologic 5.0P and 6.0P Electronic Trip Units
Micrologic 5.0H and 6.0H Electronic Trip Units
Micrologic 5.0P and 6.0P Electronic Trip Units
Micrologic 5.0H and 6.0H Electronic Trip Units
Released for:Schneider Electric Australia
Attachment(s)
Explore more
Range:
Explore more
Range: