{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What are the replacement spring charging motors for the Masterpact NT and NW?

Product Line:
Masterpact NT, Masterpact NW

Resolution:
Spring Charging Motor (MCH)
VoltageT-FrameW- & Y-Frame
FixedDrawoutFixedDrawout
AC
48S47391S47461S48207S48522
100–130S47395S47465S48211S48526
200–240S47396S47466S48212S48527
277S47398S47468S48213S48528
380–415S47398S47468S48214S48529
440–480S47400S47470S48215S48530
DC
24–30S47390S47460S48206S48521
48–60S47391S47461S48207S48522
100–130S47392S47462S48208S48523
200–250S47393S47463S48209S48524


See instruction bulletins,
Spring Charging Motor (MCH) for Masterpact® NT, Electrically-operated P-frame and NS630b–NS1600 Circuit Breakers
48049-236-01
Spring-charging Motor (MCH) for Masterpact® NW Circuit Breakers
48049-149-02

NW
NW Spring charging motor

NT
NT spring charging motor

Schneider Electric Australia