{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can I replace the MES108 Input/Output module with the MES114 module?
Yes, for Sepam 1000+ and series 20 and 40, the MES108 module reference 59645 is replaced by the MES114 module reference 59646.

The MES114 module is installed in its place. The relay will require re-configuration via SFT2841 software to accept the new Input/Output module.

The MES114 module has the following characteristics: 10 inputs, 4 outputs, power supply: 24 to 250 VDC.

Schneider Electric Australia