{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can you provide any information referencing reliability and probability of failure for the 9001KR1UH13 and 9001KR9P35RH25 devices?

Issue:
Can you provide any mean time to failure or reliability information for the  9001K/SK/KX 30 mm Push Buttons?

Product Line:
Signaling units 30mm Harmony 9001SK/K/KX push buttons, pilot lights

Environment:
Unique to the Control and signaling Units 30mm Harmony, Control and signaling XB4/XB5 Push buttons and pilot lights

Cause:
Operation not specified.

Resolution
This device is an electro-mechanical device, it has only been tested for the mechanical operations. The information regarding electrical reliability cannot be provided without knowing exactly how many electrical operations these devices will be subjected to. In theory, these devices will remain functional for an extended period without being depressed but each electrical operation is specific to their function and implementation.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: