{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can the remote racking devices (NTMPRRT and NWMPRRT) for Masterpact NT and NW be used on IEC breakers and cradles?

Issue:
Can the remote racking devices (NTMPRRT and NWMPRRT) for Masterpact NT and NW be used on IEC breakers and cradles?

Product Line:
Masterpact NT and NW

Resolution:
Yes, the racking devices can be used on IEC cradles as well as UL and ANSI versions.

Schneider Electric Australia