{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What does the SLC suffix indicate on a safety switch?
Issue:
Safety Switch SLC Suffix.

Product Line:
Safety Switch

Resolution:
The SLC suffix is used to provide a factory special safety switch with terminal lugs that accept only copper wire. The standard lugs provided on a safety switch will accept either aluminum or copper wire. This special feature is only available on type 1, 3R, 4/4X/5 stainless steel, 12/3R, and 12K switches from 30 - 600 A.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.